Hello everybody
I'm working with a SABRESD board.
First I installed LTIB from BSP L3..., then I have also managed to bring uboot, image and rootfs to an SD card, Linux starts and I can login myself with the user name root and an empty password, in LTIB I have added the package inetd and I also set the network parameters (start networking in LTIB configuration):
root@freescale /etc$ ifconfig
eth0 Link encap:Ethernet HWaddr 00:04:9F:02:6A:66
inet addr:192.168.0.222 Bcast:192.168.0.255 Mask:255.255.255.0
UP BROADCAST RUNNING MULTICAST MTU:1500 Metric:1
RX packets:0 errors:0 dropped:0 overruns:0 frame:0
TX packets:0 errors:0 dropped:0 overruns:0 carrier:0
collisions:0 txqueuelen:1000
RX bytes:0 (0.0 B) TX bytes:0 (0.0 B)
lo Link encap:Local Loopback
inet addr:127.0.0.1 Mask:255.0.0.0
UP LOOPBACK RUNNING MTU:16436 Metric:1
RX packets:0 errors:0 dropped:0 overruns:0 frame:0
TX packets:0 errors:0 dropped:0 overruns:0 carrier:0
collisions:0 txqueuelen:0
RX bytes:0 (0.0 B) TX bytes:0 (0.0 B)
root@freescale /etc$
First question: It is possible to ping the Board, but I cannot link via telnet:
Trying 192.168.0.222
Connected to 192.168.0.222.
Escape character is '^]'.
telnetd: invalid option -- 'i'
telnetd: unknown command line option: ?
Connection closed by foreign host.
What is wrong?
### Second question: How can I change the default username/password or add another user, is this possible in LTIB or kernel? How can I change the freescale in the prompt? (I need a customized user/password/prompt, I want copy this via an image to different SD cards)
### Third question: Is Yocto the better way compared to LTIB
Many thanks in advance,
Tom
Hi,
First question: It is possible to ping the Board, but I cannot link via telnet:
Trying 192.168.0.222
Connected to 192.168.0.222.
Escape character is '^]'.
telnetd: invalid option -- 'i'
telnetd: unknown command line option: ?
Connection closed by foreign host.
What is wrong?
Change following line in /etc/inetd.conf from
"Telnet stream tcp nowait root / usr / sbin / telnetd telnetd-i"
to
"Telnet stream tcp nowait root / usr / sbin / telnetd telnetd"
Regards,
Jayaram