Can i use MCU bootloader for i.MX RT1172 controller ?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Can i use MCU bootloader for i.MX RT1172 controller ?

2,456 Views
Shiva-2022
Contributor III

Hello Support Team,

 

We are working on i.MXRt1172 micro, and we wanted to use the MCU bootloader for flashing the Ext. Serial NAND Flash on custom board.

Can we use MCU bootloader which is available in below link ?

Shiva2022_0-1665499085931.png

https://www.nxp.com/design/software/development-software/mcuxpresso-software-and-tools-/mcu-bootload...

 

Please suggest.

Thank you.

 

0 Kudos
Reply
4 Replies

2,415 Views
CarlosGarabito
NXP TechSupport
NXP TechSupport

You can use the MCUBootUtility (https://github.com/JayHeng/NXP-MCUBootUtility) too for that

 

Best Regards

0 Kudos
Reply

2,447 Views
jay_heng
NXP Employee
NXP Employee

It is now available in \SDK_2.x.x_MIMXRT1170-EVK\boards\evkmimxrt1170\bootloader_examples\flashloader.

It can help to flash serial NAND.

0 Kudos
Reply

2,438 Views
Shiva-2022
Contributor III
Hello jay_heng,

Can i use blhost.exe which is present in Flashloader i.MX-RT1050 package to communicate with \SDK_2.x.x_MIMXRT1170-EVK\boards\evkmimxrt1170\bootloader_examples\flashloader ?

Please suggest.
Thank you.
0 Kudos
Reply

2,441 Views
Shiva-2022
Contributor III

Hello jay_heng,

 

Thanks for the inputs.

As suggested i have imported the bootloader project MCUXpresso.

From the bootloader project description i have understood that we need to use some utility to communicate with bootloader via serial communication.

Can you please let me know the which utilities I need to use and where I can find them?

attached the bootoader example description FYR.

 

Thank you.

0 Kudos
Reply