Can i use MCU bootloader for i.MX RT1172 controller ?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Can i use MCU bootloader for i.MX RT1172 controller ?

2,370件の閲覧回数
Shiva-2022
Contributor III

Hello Support Team,

 

We are working on i.MXRt1172 micro, and we wanted to use the MCU bootloader for flashing the Ext. Serial NAND Flash on custom board.

Can we use MCU bootloader which is available in below link ?

Shiva2022_0-1665499085931.png

https://www.nxp.com/design/software/development-software/mcuxpresso-software-and-tools-/mcu-bootload...

 

Please suggest.

Thank you.

 

0 件の賞賛
返信
4 返答(返信)

2,329件の閲覧回数
CarlosGarabito
NXP TechSupport
NXP TechSupport

You can use the MCUBootUtility (https://github.com/JayHeng/NXP-MCUBootUtility) too for that

 

Best Regards

0 件の賞賛
返信

2,361件の閲覧回数
jay_heng
NXP Employee
NXP Employee

It is now available in \SDK_2.x.x_MIMXRT1170-EVK\boards\evkmimxrt1170\bootloader_examples\flashloader.

It can help to flash serial NAND.

0 件の賞賛
返信

2,352件の閲覧回数
Shiva-2022
Contributor III
Hello jay_heng,

Can i use blhost.exe which is present in Flashloader i.MX-RT1050 package to communicate with \SDK_2.x.x_MIMXRT1170-EVK\boards\evkmimxrt1170\bootloader_examples\flashloader ?

Please suggest.
Thank you.
0 件の賞賛
返信

2,355件の閲覧回数
Shiva-2022
Contributor III

Hello jay_heng,

 

Thanks for the inputs.

As suggested i have imported the bootloader project MCUXpresso.

From the bootloader project description i have understood that we need to use some utility to communicate with bootloader via serial communication.

Can you please let me know the which utilities I need to use and where I can find them?

attached the bootoader example description FYR.

 

Thank you.

0 件の賞賛
返信