Can i.MX6x boot from 4kB page size SLC NAND?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Can i.MX6x boot from 4kB page size SLC NAND?

Jump to solution
1,742 Views
satoshishimoda
Senior Contributor I

Hi all,

I know i.MX25, i.MX35, i.MX51, and i.MX53 cannot boot from 4k byte page size SLC NAND.

Then, how about i.MX6 series (except SoloLite)?

Can i.MX6x boot from 4k byte (or larger) page size SLC NAND?

Best Regards,

Satoshi Shimoda

Labels (5)
Tags (1)
0 Kudos
Reply
1 Solution
1,365 Views
Yuri
NXP Employee
NXP Employee

Yes, the i.MX6 NAND controller GPMI is very flexible

View solution in original post

0 Kudos
Reply
4 Replies
1,365 Views
Yuri
NXP Employee
NXP Employee

The i.MX6 supports the following boot devices :
"Raw NAND (MLC and SLC), and Toggle-mode NAND flash through GPMI-2

interface. Page sizes of 2 Kbyte, 4 Kbyte and 8 Kbyte. Bus widths of 8-bit..."

0 Kudos
Reply
1,365 Views
satoshishimoda
Senior Contributor I

Dear Yuri,

Yes, i.MX6 reference manual explain i.MX6 support them.

However, i.MX25, 35, 51, and 53 could not boot from 4kB page size SLC NAND even though reference manual of each device say support it.

So I want to confirm whether all combination (SLC or MLC) && (2K byte, 4K byte, 8K byte) is no problem.

Could you confirm it?

Best Regards,

Satoshi Shimoda

0 Kudos
Reply
1,366 Views
Yuri
NXP Employee
NXP Employee

Yes, the i.MX6 NAND controller GPMI is very flexible

0 Kudos
Reply
1,365 Views
satoshishimoda
Senior Contributor I

Dear Yuri,

Our customer want to the answer.

Could you let me know it?

Best Regards,

Satoshi Shimoda

0 Kudos
Reply