Can i.MX6 boot with no attached DDR?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Can i.MX6 boot with no attached DDR?

899 次查看
michaeln
Contributor I

Hi Everyone,

Newbie here.  My team has asked if an i.MX6 can boot with no DDR attached,

and I'm having problems finding the info in any of the documents.

Thanks,

Mike

标签 (1)
0 项奖励
回复
1 回复

830 次查看
Yuri
NXP Employee
NXP Employee

Hello,

  it is possible to load / boot and run relatively simple application to internal

memory (OCRAM) of the i.MX6 without external DDR.

Please look at an example, attached in the following thread.

Integrating Processor Expert for i.MX and ARM GCC with Eclipse


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复