Can different devices connect to i.MX6 same I2S interface?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Can different devices connect to i.MX6 same I2S interface?

Jump to solution
1,456 Views
satoshishimoda
Senior Contributor I

Hi community,

I have a question about i.MX6 audio connection.

I want to know whether i.MX6 can control if different devices (DAC & ADC) are connected to TX and RX of same I2S interface as attached image.

I think it is no-problem, right?

I2S_Connection.png

Best Regards,

Satoshi Shimoda

Labels (6)
Tags (2)
0 Kudos
Reply
1 Solution
1,332 Views
saurabh206
Senior Contributor III

Hi

Satoshi

It should work, but at a time only one device should be active, due to clocking issue.

If both device are used as a slave mode and operates on same frequency than it should work together.

Thanks

Saurabh

View solution in original post

0 Kudos
Reply
2 Replies
1,332 Views
igorpadykov
NXP Employee
NXP Employee

Hi Satoshi

you are right, this should be no problem.

Best regards

igor

1,333 Views
saurabh206
Senior Contributor III

Hi

Satoshi

It should work, but at a time only one device should be active, due to clocking issue.

If both device are used as a slave mode and operates on same frequency than it should work together.

Thanks

Saurabh

0 Kudos
Reply