Can different devices connect to i.MX6 same I2S interface?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Can different devices connect to i.MX6 same I2S interface?

跳至解决方案
2,110 次查看
satoshishimoda
Senior Contributor I

Hi community,

I have a question about i.MX6 audio connection.

I want to know whether i.MX6 can control if different devices (DAC & ADC) are connected to TX and RX of same I2S interface as attached image.

I think it is no-problem, right?

I2S_Connection.png

Best Regards,

Satoshi Shimoda

标签 (6)
标记 (2)
0 项奖励
回复
1 解答
1,986 次查看
saurabh206
Senior Contributor III

Hi

Satoshi

It should work, but at a time only one device should be active, due to clocking issue.

If both device are used as a slave mode and operates on same frequency than it should work together.

Thanks

Saurabh

在原帖中查看解决方案

0 项奖励
回复
2 回复数
1,986 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Satoshi

you are right, this should be no problem.

Best regards

igor

1,987 次查看
saurabh206
Senior Contributor III

Hi

Satoshi

It should work, but at a time only one device should be active, due to clocking issue.

If both device are used as a slave mode and operates on same frequency than it should work together.

Thanks

Saurabh

0 项奖励
回复