Can IMX8ulp MIPI-DSI support 720P

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Can IMX8ulp MIPI-DSI support 720P

1,994件の閲覧回数
zlxie
Contributor I

Can IMX8ulp's  4 lanes MIPI-DSI support 720P (720 X 3 RGB X 1280)  at 60 frames per second? if not, what frame speed can be supported? 30, 20 ,15 or less? Thanks.

0 件の賞賛
返信
2 返答(返信)

1,977件の閲覧回数
Sanket_Parekh
NXP TechSupport
NXP TechSupport

Hello @zlxie,

I hope you are doing well.

Please refer to Chapter 61 MIPI-DSI Host Controller (MIPI-DSI) from the link below.
https://www.nxp.com/docs/en/reference-manual/IMX8ULPRM.pdf

It will help you

Thanks & Regards,
Sanket Parekh

0 件の賞賛
返信

1,974件の閲覧回数
gary_bisson
Senior Contributor III

Hi,

That doesn't answer the question though. The chapter only mentions:

"This module does not support the 74.25 MHz pixel clock rate generation for 720p60 and 1080p30 resolutions."

But it doesn't say the maximum pixel clock supported and therefore what framerate can be achieved at 720p (45fps)?

Regards,

Gary

0 件の賞賛
返信