Can IMX8ulp MIPI-DSI support 720P

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Can IMX8ulp MIPI-DSI support 720P

985 Views
zlxie
Contributor I

Can IMX8ulp's  4 lanes MIPI-DSI support 720P (720 X 3 RGB X 1280)  at 60 frames per second? if not, what frame speed can be supported? 30, 20 ,15 or less? Thanks.

0 Kudos
Reply
2 Replies

968 Views
Sanket_Parekh
NXP TechSupport
NXP TechSupport

Hello @zlxie,

I hope you are doing well.

Please refer to Chapter 61 MIPI-DSI Host Controller (MIPI-DSI) from the link below.
https://www.nxp.com/docs/en/reference-manual/IMX8ULPRM.pdf

It will help you

Thanks & Regards,
Sanket Parekh

0 Kudos
Reply

965 Views
gary_bisson
Senior Contributor III

Hi,

That doesn't answer the question though. The chapter only mentions:

"This module does not support the 74.25 MHz pixel clock rate generation for 720p60 and 1080p30 resolutions."

But it doesn't say the maximum pixel clock supported and therefore what framerate can be achieved at 720p (45fps)?

Regards,

Gary

0 Kudos
Reply