Can IMX6 fix the sample rate before output from I2S

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Can IMX6 fix the sample rate before output from I2S

787 次查看
jane-jiajuan_zh
Contributor III

Hi, 

My board use imx6solo, and the codec chipset is only support the 8K sample rate. so we hope to fix the sample rate before IMX6 output from I2S.

We tried gstreamer re-sample pipeline, and it works. But we hope to find a hardware way to support it.

Is that possible by any hardware module to fix the sample rate?

Best Regards,

Jane

0 项奖励
回复
1 回复

752 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Jane

i.MX6Q has ASRC module for such purpose, so one can check ASRC driver description

in Linux Manual included in Linux 4.19.35_1.1.0 Documentation

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复