Can I use DMA in DM Core?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Can I use DMA in DM Core?

846 Views
hiromichimatsum
Contributor II

Dear all,

I can see DMA block in "DM Core Block Diagram".

This diagram is on "i.MX6D/Q Reference Manual".

The figure is "Figure 48-1. DM Core Block Diagram" at p.4054 in the Reference Manual Rev. 1, 04/2013.

Can I use this DMA in DM Core?

I believe that this DMA can be used in EP mode at least.

But there is no details in the Reference Manual regarding above matter.

I'd like to thank if you can show me the relevant document or the specification for the DMA in DM Core?

Best regards,

Hiromichi

Labels (1)
0 Kudos
Reply
0 Replies