Can FelxSPI bus be used for regular, non-flash-memory SPI devices?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Can FelxSPI bus be used for regular, non-flash-memory SPI devices?

632 Views
oliverco
Contributor I

I need add'l SPI buses beyond the SPI1, SP2 and SP3 offered, and I thought FlexSPI should be possible to be used as a regular single-lane SPI bus?

0 Kudos
Reply
1 Reply

606 Views
Manuel_Salas
NXP TechSupport
NXP TechSupport

Hello @oliverco 

 

FlexSPI is primarily designed for interfacing with NOR/NAND Flash memory devices, but you can use it to interface other kind of SPI devices, but you should modify the device tree and maybe the driver for FleSPI.

Maybe it is preferible to use the SPI peripheral directly.

Also you can test if FlexSPI works with your device with spidev_test.

 

Best regards,

--... ...--

Salas.

0 Kudos
Reply