Can FelxSPI bus be used for regular, non-flash-memory SPI devices?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Can FelxSPI bus be used for regular, non-flash-memory SPI devices?

624件の閲覧回数
oliverco
Contributor I

I need add'l SPI buses beyond the SPI1, SP2 and SP3 offered, and I thought FlexSPI should be possible to be used as a regular single-lane SPI bus?

ラベル(1)
0 件の賞賛
返信
1 返信

598件の閲覧回数
Manuel_Salas
NXP TechSupport
NXP TechSupport

Hello @oliverco 

 

FlexSPI is primarily designed for interfacing with NOR/NAND Flash memory devices, but you can use it to interface other kind of SPI devices, but you should modify the device tree and maybe the driver for FleSPI.

Maybe it is preferible to use the SPI peripheral directly.

Also you can test if FlexSPI works with your device with spidev_test.

 

Best regards,

--... ...--

Salas.

0 件の賞賛
返信