Cameras on IMX53

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Cameras on IMX53

3,530 次查看
PeterKhrapchenk
Contributor I

Hi,

In my project i need two cameras working simultaneously on a chip(just like 3d cameras). Does IMX53 support this mode by default or not? If not, how can i implement this?

Best regards,

Peter.

标记 (1)
0 项奖励
回复
6 回复数

3,219 次查看
paulhottell
Contributor I

Hello,

Has anyone had any luck finding a patch for multiple CSI support? I am currently trying to get this functionality working myself. I've seen several threads talking about it, but haven't seen any patches posted.

Any assistance would be greatly appreciated!

Regards,

Paul

0 项奖励
回复

3,219 次查看
HenriBragge
Fresh Out Contributor

Hi Marko,

Did you have success modifying mxc_v4l2_capture.c? Probably some tips or even patches that you could share?

Thanks.

0 项奖励
回复

3,219 次查看
MarkoPanger
Contributor III

I'm also working on a project wich requires two cameras. We plan to connect them through CSI0 and CSI1. So far no problems. From the HW point of view is an rather easy task. However the current IPU driver provided y freescale doesn't support usage of two cameras. The file mxc_v4l2_capture.c supports only one instance and has to be modified along with other stuff probably. I plan to work on that in the next few weeks.

Please update us on your progress.

Marko

0 项奖励
回复

3,219 次查看
ff
Contributor II

hi Marko

  recently I'm  also working on a project with requires two cameras,

would u please show us your achievement on this project?

best regards

0 项奖励
回复

3,219 次查看
AndrejBarbis
Contributor I

it is possible to connect two CSI cameras on iMX53 Quick Start Board on the CSI0 and CSI1? Camera has 12-bits. I would like to use QSH-060-01 connector, which support CSI0 (only 8-bits) and i don't need DISP0 pins, which i want to use for connecting second camera, if it's possible. I know, that iMX53 support CSI0 for connecting first camera and CSI1 for connecting second camera.

 

Best regards,

 

Andrej 

0 项奖励
回复

3,219 次查看
daiane_angolini
NXP Employee
NXP Employee

iMX53 can handle up to 2 CSI cameras (hardware acceleration input), although you will need to prepare some hardware for that.

 

You can work with 2 USB cameras, in this case, you can you QSB as is, and have your stereo camera.

 

So, please, describe the hardware you´ve been using for that.

0 项奖励
回复