Camera issue IMX8QXP C0

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Camera issue IMX8QXP C0

10,763 Views
ShivM
Contributor II

We have a custom hardware board based on i.MX8QXP SoC. Connected to it is the Sony imx215 camera that output image in RAW10 format.

We have few questions as below:

(1)

When these pixel values are received from ISI as 16-bit, the 10-bit value from RAW10 format is placed in it as 00XX XXXX XXXX 0000, where X is one bit of the color value. Hence in the application, received 16-bit value is shifted right by 4. Also, since application treats resulting 16-bit value as 16-bit color sample, value is scaled to 16-bit from 10-bit. (i. e. multiply by 65535.0/1023).

For a sample, output captured from ISI when test pattern is enabled in imx215.

Refer Without code changes in application RAW.png and  With code changes in application for RAW.png

In case "Without code changes in application RAW.png " above, bits are lost in color values when captured from ISI. Case "With code changes in application for RAW.png" shows correct results when code changes were made in application not to lose bits.

We would like to know if there is a way to avoid shifting bits or do it in hardware or GPU? (To avoid the overhead caused to application because of above).

(2)

It looks like the output image from camera is very low in brightness and overall appearance that it requires gamma correction and/or white balance to get a good picture.

A sample is below.

Refer "Without code changes in application.png" and "With code changes in application, brightness and color values enhanced in windows photo application.png"

Is there any support from hardware to perform such operations?

0 Kudos
Reply
2 Replies

10,728 Views
joanxie
NXP TechSupport
NXP TechSupport

i.mx8qxp ISI has shift issue when capture raw data, but C0 version fixed this, pls refer to the attached document, do you mean you still get the issue on C0 board? if yes, could you tell me what your imx8qxp part number is?

0 Kudos
Reply

10,731 Views
ShivM
Contributor II

Can someone pls respond to this question?

0 Kudos
Reply