Camera image stopping issue in IMX356

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Camera image stopping issue in IMX356

1,242件の閲覧回数
hyun-moyang
Contributor III

Hi All,

I used IMX356 chipset and video chipset(MAX9526)

In camera preview state, when camera connector is abnormal case, if video chipset(MAX9526) generate the video signal or not  several times, Camera preview image  is stopped in LCD screen in IMX356, or Camera preview image is displayed abnormally in IMX356

please help me to resolve this issue

タグ(1)
0 件の賞賛
返信
2 返答(返信)

1,091件の閲覧回数
hyun-moyang
Contributor III

Hi Igor,

Our BSP Version is Linux-2.6.31 and u-boot.2009.08, and we used the IMX356 chipset.

And Video Chipset of Our Camera is MAX9526,Video Signal is CVBS and BT656.

Regards

HM

0 件の賞賛
返信

1,091件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Hyun-mo

please try suggestion for implementing new camera driver given in

Chapter 19 Supporting the i.MX53 Camera Sensor Interface CSI0

i.MX53 System Development User’s Guide

http://www.freescale.com/files/32bit/doc/user_guide/MX53UG.pdf

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信