Camera image stopping issue in IMX356

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Camera image stopping issue in IMX356

1,201 次查看
hyun-moyang
Contributor III

Hi All,

I used IMX356 chipset and video chipset(MAX9526)

In camera preview state, when camera connector is abnormal case, if video chipset(MAX9526) generate the video signal or not  several times, Camera preview image  is stopped in LCD screen in IMX356, or Camera preview image is displayed abnormally in IMX356

please help me to resolve this issue

标记 (1)
0 项奖励
回复
2 回复数

1,050 次查看
hyun-moyang
Contributor III

Hi Igor,

Our BSP Version is Linux-2.6.31 and u-boot.2009.08, and we used the IMX356 chipset.

And Video Chipset of Our Camera is MAX9526,Video Signal is CVBS and BT656.

Regards

HM

0 项奖励
回复

1,050 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Hyun-mo

please try suggestion for implementing new camera driver given in

Chapter 19 Supporting the i.MX53 Camera Sensor Interface CSI0

i.MX53 System Development User’s Guide

http://www.freescale.com/files/32bit/doc/user_guide/MX53UG.pdf

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复