Camera Max9286 driver issue

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Camera Max9286 driver issue

Jump to solution
4,650 Views
xu_ji1
Contributor V

Hello,

I think the i.MX8Q P9.0.0_2.1.0-AUTO-ga release camera MAX9286 driver has some problem,when I use MAX9286 and four cameras on mek board,I can only use dev/video0 camera,other cameras dev/video1 video2 and video3 can not used.

Does the driver only support one camera?How can support all four cameras?

Please give help.

Thanks

Tags (1)
0 Kudos
Reply
1 Solution
4,351 Views
igorpadykov
NXP Employee
NXP Employee

it will be fixed in new silicon revision, for schedule please

contact local marketing office.

Best regards
igor

View solution in original post

0 Kudos
Reply
9 Replies
4,351 Views
nxf47746
NXP Employee
NXP Employee

Only 8QM support 4 camera, 8QXP b0 support one.

0 Kudos
Reply
4,351 Views
xu_ji1
Contributor V

hello,

What diff 8QM with 8QXP?SW side diff or HW side limited?

Thanks

0 Kudos
Reply
4,351 Views
nxf47746
NXP Employee
NXP Employee

It is hardware limited, 8QM mipi csi2 support virtual channel, but 8QXP b0 do not support.

0 Kudos
Reply
4,351 Views
xu_ji1
Contributor V

What is 8QXP b0?In the released document both 8QM and 8QXP write:

• Stream Multiplexing
• Differentiates multiple cameras from a single 4 lane MIPI input

And from System Block Diagram diff is MIPI CSI2 1x or 2x,others no diff.

Could u explain detail about 8QXP HW limited?

Thanks

0 Kudos
Reply
4,351 Views
nxf47746
NXP Employee
NXP Employee

8QXP b0 means soc version: b0, currently 8qxp b0 mipi csi2 do not support virtual channel.

Except for virtual channel 0, virtual channels 1, 2, and 3 do not have proper VSYNC timing from MIPI CSI2 when different cameras are multiplexed together. As a result, frames stored in memory can be corrupted due to missing last lines.

This will be fixed lately.

0 Kudos
Reply
4,351 Views
xu_ji1
Contributor V

you means 8QXP will fixed it on HW side later?SW side not need changed?

And what is the fixed schedule,could u shared?

Thanks

0 Kudos
Reply
4,351 Views
igorpadykov
NXP Employee
NXP Employee

Hi Xu

one can look at errata document e50058 :

Virtual channels 1, 2, and 3 do not work normally for multiplexed cameras.

https://www.nxp.com/docs/en/errata/IMX8X_0N95W.pdf 

Best regards
igor

0 Kudos
Reply
4,351 Views
xu_ji1
Contributor V

hello,

I think it is not answer my question properly.

Fixed schedule,HW or SW side will fixed?

Thanks

0 Kudos
Reply
4,352 Views
igorpadykov
NXP Employee
NXP Employee

it will be fixed in new silicon revision, for schedule please

contact local marketing office.

Best regards
igor

0 Kudos
Reply