CSI1 data port selection

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

CSI1 data port selection

跳至解决方案
1,682 次查看
johnciple
Contributor I

Hi,

I am designing with iMX6D.

I have to connect the CSI1 and parallel Camera(8bit bayer).

EIM Ports have IPU2_CSI1_DATA0 ~ IPU2_CSI1_DATA19.

Can I select data port?

I want to use IPU2_CSI1_DATA10 ~ IPU2_CSI1_DATA17.

Because I want to avoid to overlap with BootConfig.

Is this OK?

标签 (1)
标记 (2)
0 项奖励
回复
1 解答
1,529 次查看
Yuri
NXP Employee
NXP Employee

Hello,

  Please use section 4.11.10.1 (IPU Sensor Interface Signal Mapping)

of the Datasheet about supported CSI signals connections.

http://cache.freescale.com/files/32bit/doc/data_sheet/IMX6DQCEC.pdf 


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,530 次查看
Yuri
NXP Employee
NXP Employee

Hello,

  Please use section 4.11.10.1 (IPU Sensor Interface Signal Mapping)

of the Datasheet about supported CSI signals connections.

http://cache.freescale.com/files/32bit/doc/data_sheet/IMX6DQCEC.pdf 


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复