CSI1 data port selection

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

CSI1 data port selection

ソリューションへジャンプ
2,232件の閲覧回数
johnciple
Contributor I

Hi,

I am designing with iMX6D.

I have to connect the CSI1 and parallel Camera(8bit bayer).

EIM Ports have IPU2_CSI1_DATA0 ~ IPU2_CSI1_DATA19.

Can I select data port?

I want to use IPU2_CSI1_DATA10 ~ IPU2_CSI1_DATA17.

Because I want to avoid to overlap with BootConfig.

Is this OK?

ラベル(1)
タグ(2)
0 件の賞賛
返信
1 解決策
2,079件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

  Please use section 4.11.10.1 (IPU Sensor Interface Signal Mapping)

of the Datasheet about supported CSI signals connections.

http://cache.freescale.com/files/32bit/doc/data_sheet/IMX6DQCEC.pdf 


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
2,080件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

  Please use section 4.11.10.1 (IPU Sensor Interface Signal Mapping)

of the Datasheet about supported CSI signals connections.

http://cache.freescale.com/files/32bit/doc/data_sheet/IMX6DQCEC.pdf 


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信