CS4350 Linux Driver i.MX6

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

CS4350 Linux Driver i.MX6

Jump to solution
1,829 Views
atillametetured
Contributor V

Hello,

We are having problems with CS4350, alsa insists that there are "no soundcards detected" however it is using the i2c ports when we do i2cdetect. Is there anyone with CS4350 experience that can advise us what we might be doing wrong?

Regards,

Mete

Labels (2)
0 Kudos
Reply
1 Solution
1,592 Views
atillametetured
Contributor V

Hello Carlos,

Thank you for your reply. For anyone wondering how it turned out, here is how we fixed this issue;

https://community.nxp.com/thread/447047 

Regards,

Mete

View solution in original post

0 Kudos
Reply
2 Replies
1,592 Views
Carlos_Musich
NXP Employee
NXP Employee

Hi Atilla,

these are the only drivers provided in the i.MX6 Linux image.


<build_dir>/tmp/work/cortexa9hf-vfp-neon-poky-linux-gnueabi/linux-libc-headers/3.14-r0/linux-3.14/sound/pci/oxygen/cs4362a.h
<build_dir>/tmp/work/cortexa9hf-vfp-neon-poky-linux-gnueabi/linux-libc-headers/3.14-r0/linux-3.14/sound/pci/oxygen/cs4398.h
<build_dir>/tmp/work/cortexa9hf-vfp-neon-poky-linux-gnueabi/linux-libc-headers/3.14-r0/linux-3.14/sound/pci/oxygen/xonar_cs43xx.c

If these drivers are not helpful you may contact the manufacturer of the device to ask for a Linux driver which you may add to the I.MX6 image.


Regards,
Carlos

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

1,593 Views
atillametetured
Contributor V

Hello Carlos,

Thank you for your reply. For anyone wondering how it turned out, here is how we fixed this issue;

https://community.nxp.com/thread/447047 

Regards,

Mete

0 Kudos
Reply