CS4350 Linux Driver i.MX6

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

CS4350 Linux Driver i.MX6

ソリューションへジャンプ
2,552件の閲覧回数
atillametetured
Contributor V

Hello,

We are having problems with CS4350, alsa insists that there are "no soundcards detected" however it is using the i2c ports when we do i2cdetect. Is there anyone with CS4350 experience that can advise us what we might be doing wrong?

Regards,

Mete

ラベル(2)
タグ(5)
0 件の賞賛
返信
1 解決策
2,315件の閲覧回数
atillametetured
Contributor V

Hello Carlos,

Thank you for your reply. For anyone wondering how it turned out, here is how we fixed this issue;

https://community.nxp.com/thread/447047 

Regards,

Mete

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,315件の閲覧回数
Carlos_Musich
NXP Employee
NXP Employee

Hi Atilla,

these are the only drivers provided in the i.MX6 Linux image.


<build_dir>/tmp/work/cortexa9hf-vfp-neon-poky-linux-gnueabi/linux-libc-headers/3.14-r0/linux-3.14/sound/pci/oxygen/cs4362a.h
<build_dir>/tmp/work/cortexa9hf-vfp-neon-poky-linux-gnueabi/linux-libc-headers/3.14-r0/linux-3.14/sound/pci/oxygen/cs4398.h
<build_dir>/tmp/work/cortexa9hf-vfp-neon-poky-linux-gnueabi/linux-libc-headers/3.14-r0/linux-3.14/sound/pci/oxygen/xonar_cs43xx.c

If these drivers are not helpful you may contact the manufacturer of the device to ask for a Linux driver which you may add to the I.MX6 image.


Regards,
Carlos

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

2,316件の閲覧回数
atillametetured
Contributor V

Hello Carlos,

Thank you for your reply. For anyone wondering how it turned out, here is how we fixed this issue;

https://community.nxp.com/thread/447047 

Regards,

Mete

0 件の賞賛
返信