CLKO2 output problem

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

CLKO2 output problem

Jump to solution
5,879 Views
avexwu
Contributor II

Hi there,

I am using i.MX6Q. I want to use CLKO2 as the MCLK source of my camera. The steps I did are as followed.

1.    Setup Pad , set gpio3 as clko2 output pin

MX6Q_PAD_GPIO_3__CCM_CLKO2,              // setup gpio3 as output pin of clko2

2.    get/set osc_clk as parent clock of clko2, set rate, and enable clko2

        clko2 = clk_get(NULL, "clko2_clk");

        if (IS_ERR(clko2))

                printk("can't get CLKO2 clock.\n");

        new_parent = clk_get(NULL, "osc"); // in sabresd bsp source code, "osc_clk" is a wrong name, tested already

        if (!IS_ERR(new_parent)) {

                clk_set_parent(clko2, new_parent);

                clk_put(new_parent);

        }

        rate = clk_round_rate(clko2, 24000000);

        clk_set_rate(clko2, rate);

        clk_enable(clko2);


However, there is nothing on gpio_3 pin, no clock on CLKO2 output pin. It seems the I miss some steps.

I print out the register CCOSR,  MXC_CCM_CCOSR=0x010E000F (1 00001110 00000000 00001111)

It seems the value is correctly be set, but it did not function as it should be.

The same way I used is okay to enable/disable CLKO, any idea? I use SABRESD android bsp as my source code base.

thanks anyway

avex

Labels (1)
0 Kudos
Reply
1 Solution
5,017 Views
avexwu
Contributor II

Just see this my old post.

Answer to myself , YES, it's a bug but not hardware.

View solution in original post

0 Kudos
Reply
9 Replies
5,017 Views
emilmyhrman
Contributor IV

I'm having the same problem. What was the bug you found?

regards,

Emil

0 Kudos
Reply
5,017 Views
emilmyhrman
Contributor IV

Figured it out. Register IOMUXC_SW_PAD_CTL_PAD_GPIO03 is set wrong when using the macro MX6Q_PAD_GPIO_0__CCM_CLKO.


Change it to "IOMUX_PAD(0x05F8, 0x0228, 4, 0x0000, 0, MX6DL_CCM_CLK0_PAD_CTRL)" and it should work.

0 Kudos
Reply
5,017 Views
rohanbhargava
Contributor I

How do I do this? I have been looking around but can't find the exact file to set this.

Could you please provide detailed instructions?

Thanks

0 Kudos
Reply
5,017 Views
fangmingan
Contributor I

dear avex& weidong,

   I encounter the same situation as you. But i didn't understand your solution? how did you fix the bug? avexwu weidong.sun

thanks a lot

Fangming

0 Kudos
Reply
5,018 Views
avexwu
Contributor II

Just see this my old post.

Answer to myself , YES, it's a bug but not hardware.

0 Kudos
Reply
5,017 Views
avexwu
Contributor II

Anyone can help?

Is it a bug of i.MX6Q CPU?

0 Kudos
Reply
5,017 Views
weidong_sun
NXP TechSupport
NXP TechSupport

Hello,Avex,

Would you like to try like the following steps ?

(1)IOMUX ( what you did is correct)

(2)Make 24M clock output via GPIO_3 PIN

clk_set_parent(&clko2_clk,&osc_clk);

clk_set_rate(&clko2_clk,24000000);

Regards,

Weidong

0 Kudos
Reply
5,017 Views
avexwu
Contributor II

Hi Weidong,

thanks for your reply,

1. There are two clock out of i.MX6Q, clko and clko2. clko works fine, and its IOMUX is MX6Q_PAD_GPIO_0__CCM_CLKO

I am working on clko2 , IOMUX is as step 1 of my post listed above.

2. As step 2 of my post above, I use osc_clk at 24MHZ already.

Regards,

0 Kudos
Reply
5,017 Views
weidong_sun
NXP TechSupport
NXP TechSupport

OK, good job !

Regards,

Weidong

0 Kudos
Reply