CCM_ANALOG_MISC2 cannot be configured

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

CCM_ANALOG_MISC2 cannot be configured

2,508 次查看
chrisolarti
Contributor I

Hi Freescale,

I am trying to use the CCAM_ANALOG_MISC2:AUDIO_DIV_MSB, AUDIO_DIV_LSB so I can divide the PLL4_AUDIO clock (pll4_main_clock) from 688.128MHz to 86.016MHz.  I can verify the PLL4_AUDIO is reaching to 688.128MHz when using CCM_ANALOG_PLL_AUDIOn:DIV_SELECT=28, CCM_ANALOG_PLL_AUDIO_NUM=672, CCM_ANALOG_PLL_AUDIO_DENOM=1000.  This is following equation with Fref=24MHz:

pastedImage_144.png

I can also verify the CCM_ANALOG_PLL_AUDIOn:POST_DIV_SELECT=0 (divide by 4) is working to give a pll4_main_clock=172.032MHz.  However, when trying to configure CCM_ANALOG_MISC2:AUDIO_DIV_MSB & AUDIO_DIV_LSB to divide by 2:

pastedImage_423.png

I do not see the pll4_main_clock=86.016MHz.

My observation is using CCM_CCOSR:CCM_CLKO1 to use PLL4_MAIN_CLK as the source clock with a divider by 1.

I also took note in CCM_ANALOG_MISC2:AUDIO_DIV_MSB where the: output clock of the audio PLL should be "gated" prior to changing this divider to prevent glitches. However when configuring CCM_ANALOG_PLL_AUDIOn:POWERDOWN=1 during ENABLED=1/BYPASS=1, I am unable to get the PLL to enter a DEACTIVE HIGH STATE, which should make the PLL "gated". 

I tried with with CCM_ANALOG_PLL_VIDEO and that seems to be working fine.

My order for switching PLL speeds at reset:

1. BYPASS = 0 --> (POWERDOWN will remain = 1 & ENABLE will be = 0)

2. CONFIGURE PLL DIV_SELECT, NUMERATOR, DENOMINATOR, MISC2

3. ENABLE = 1

4. POWERDOWN = 0

5. WAIT WHILE CCM_ANALOG_PLL_AUDIO:LOCK = 1

Is there anything else that I am missing when trying to "gate" PLL4_AUDIO?  Or is PLL4_AUDIO is unable to be "gated" since there is no CCGR for pll4_main_clk?

Thanks in advance.

Chris.

标签 (1)
0 项奖励
回复
6 回复数

2,212 次查看
igorpadykov
NXP Employee
NXP Employee

Hi chris

suggest also to try "10" - divide by 1

and use for that i.MX 6Series Platform SDK

and look at EB790 Configuration of Phase Fractional Dividers

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

2,212 次查看
bonzo
NXP Employee
NXP Employee

See this post.  https://community.freescale.com/thread/328512?q=PLL4%20AUDIO_DIV

It seems that for iMX6D/Q, "CCM_ANALOG_MISC2n[MSB:LSB]" divider does NOT exist.

0 项奖励
回复

2,212 次查看
chrisolarti
Contributor I

I am unable to access that link.  Can I have privileges to review?

Thank you.

Chris.

0 项奖励
回复

2,211 次查看
bonzo
NXP Employee
NXP Employee

See attached.

Brad

0 项奖励
回复

2,211 次查看
keitanagashima
Senior Contributor I

Dear Bradley,

Hello. My customer faced the same issue (i.e. He wasn't able to configure the AUDIO_DIV_LSB and MSB).

(Device : i.MX 6Quad)

You said ; CCM_ANALOG_MISC2n[MSB:LSB]" divider does NOT exist.

Really?

I checked the latest reference manual and chip errata today.

But, the related description wasn't found!

Best Regards,

Keita

0 项奖励
回复

2,211 次查看
igorpadykov
NXP Employee
NXP Employee

Thanks Bradley for pointing on that !

Best regards

Igor

0 项奖励
回复