CAN FD on iMX6ULL

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

CAN FD on iMX6ULL

Jump to solution
4,497 Views
carlesre
Contributor II

Dear all,

I've find lot of contradictory information about the possibility to use CAN FD devices with iMX6 processors.

Some comments on this forum dated 2015 clearly say that they are not compatible, while Flex CAN definition says it is completely compatible.

Could anybody CONFIRM that CAN FD can be used on any iMX6 processor?

Please identify which are compatible and which are not. I am interested on iMX6ULL but I could use any other family

Thank you very much

Labels (2)
Tags (3)
0 Kudos
Reply
1 Solution
4,183 Views
gusarambula
NXP TechSupport
NXP TechSupport

Hello Carles Recasens,

My apologies for the delay and the confusion. I confirmed that the i.MX6ULL FlexCan does not have FD support.

Regards,

View solution in original post

0 Kudos
Reply
3 Replies
4,184 Views
gusarambula
NXP TechSupport
NXP TechSupport

Hello Carles Recasens,

My apologies for the delay and the confusion. I confirmed that the i.MX6ULL FlexCan does not have FD support.

Regards,

0 Kudos
Reply
4,048 Views
ankith
Contributor I

Hi

Is it not compatible only with iMX6ULL series or all iMX6 devices. I wanted same info on iMX6QP board, Any input will be helpful.

Thank you,

0 Kudos
Reply
4,183 Views
carlesre
Contributor II

Thank you

0 Kudos
Reply