CAN FD on iMX6ULL

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
4,482件の閲覧回数
carlesre
Contributor II

Dear all,

I've find lot of contradictory information about the possibility to use CAN FD devices with iMX6 processors.

Some comments on this forum dated 2015 clearly say that they are not compatible, while Flex CAN definition says it is completely compatible.

Could anybody CONFIRM that CAN FD can be used on any iMX6 processor?

Please identify which are compatible and which are not. I am interested on iMX6ULL but I could use any other family

Thank you very much

ラベル(2)
タグ(3)
0 件の賞賛
返信
1 解決策
4,168件の閲覧回数
gusarambula
NXP TechSupport
NXP TechSupport

Hello Carles Recasens,

My apologies for the delay and the confusion. I confirmed that the i.MX6ULL FlexCan does not have FD support.

Regards,

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
4,169件の閲覧回数
gusarambula
NXP TechSupport
NXP TechSupport

Hello Carles Recasens,

My apologies for the delay and the confusion. I confirmed that the i.MX6ULL FlexCan does not have FD support.

Regards,

0 件の賞賛
返信
4,033件の閲覧回数
ankith
Contributor I

Hi

Is it not compatible only with iMX6ULL series or all iMX6 devices. I wanted same info on iMX6QP board, Any input will be helpful.

Thank you,

0 件の賞賛
返信
4,168件の閲覧回数
carlesre
Contributor II

Thank you

0 件の賞賛
返信