CAAM API integration with U-Boot

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

CAAM API integration with U-Boot

2,486 次查看
kanimozhi_t
Contributor V

Hi,

    We would like to use CAAM for hash calculation and comparison on U-Boot. We know that we can use HAB APIs to utilise the CAAM internally but we're interested in using the CAAM directly for the above mentioned tasks.

    1. Is CAAM API available for public use? If so, where can we find the documentation?

    2. How can we integrate CAAM API on U-Boot? Are there any examples?

Any suggestions would highly be appreciated.

标签 (4)
标记 (3)
0 项奖励
回复
3 回复数

2,468 次查看
Yuri
NXP Employee
NXP Employee

@kanimozhi_t 
Hello,

  we do not support CAAM API for U-boot. Only Linux interface is available.

Regards,
Yuri.

2,463 次查看
kanimozhi_t
Contributor V

Thank you @Yuri for the quick update.

 

BTW, can you share the links for CAAM Linux API?

2,453 次查看
Yuri
NXP Employee
NXP Employee

@kanimozhi_t 
Hello,

    please refer to Chapter 8 (Security) of the NXP Linux RM.

https://www.nxp.com/docs/en/reference-manual/IMX_REFERENCE_MANUAL.pdf

 

Regards,
Yuri.