CAAM API integration with U-Boot

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

CAAM API integration with U-Boot

3,194件の閲覧回数
kanimozhi_t
Contributor V

Hi,

    We would like to use CAAM for hash calculation and comparison on U-Boot. We know that we can use HAB APIs to utilise the CAAM internally but we're interested in using the CAAM directly for the above mentioned tasks.

    1. Is CAAM API available for public use? If so, where can we find the documentation?

    2. How can we integrate CAAM API on U-Boot? Are there any examples?

Any suggestions would highly be appreciated.

ラベル(4)
タグ(3)
0 件の賞賛
返信
3 返答(返信)

3,176件の閲覧回数
Yuri
NXP Employee
NXP Employee

@kanimozhi_t 
Hello,

  we do not support CAAM API for U-boot. Only Linux interface is available.

Regards,
Yuri.

3,171件の閲覧回数
kanimozhi_t
Contributor V

Thank you @Yuri for the quick update.

 

BTW, can you share the links for CAAM Linux API?

3,161件の閲覧回数
Yuri
NXP Employee
NXP Employee

@kanimozhi_t 
Hello,

    please refer to Chapter 8 (Security) of the NXP Linux RM.

https://www.nxp.com/docs/en/reference-manual/IMX_REFERENCE_MANUAL.pdf

 

Regards,
Yuri.