BusFreq IMX driver in mainline kernel?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

BusFreq IMX driver in mainline kernel?

5,985 Views
Harvie
Contributor II

Hello

are there any chances of getting busfreq driver running on mainline kernel?

it seems to me that i am not able to reliably run UART at speeds higher than 1M baud without it... (i am looking for 3M baud serial communication)

Labels (2)
Tags (1)
0 Kudos
Reply
7 Replies

5,950 Views
joanxie
NXP TechSupport
NXP TechSupport

pls refer to the chapter  2.5.4 Dynamic Bus Frequency of enclosed file

0 Kudos
Reply

5,945 Views
Harvie
Contributor II

Thank you. I've read everything in that chapter, unfortunately that does not explain my issues with serial communication using mainline kernel...

0 Kudos
Reply

5,921 Views
joanxie
NXP TechSupport
NXP TechSupport

what processors do you use? did you have this issue on nxp bsp? what's your mainline version?

0 Kudos
Reply

5,889 Views
Harvie
Contributor II

Hello,

IC package says MIMX8MM6CV1KZAA,

i've tried several mainline versions. Mostly 5.15.18,

with BSP kernel i do not have this issue.

 

 

0 Kudos
Reply

5,864 Views
joanxie
NXP TechSupport
NXP TechSupport

since you test nxp bsp successfully, I couldn't reproduce this issue on my side, could you share more detailed information about your issue, let me check if we have patch or anything else useful information for you, but we don't maintain mainline kernel

0 Kudos
Reply

5,693 Views
Harvie
Contributor II

Ok, i think the problem is that

/sys/class/tty/ttymxc0/uartclk = 24000000 Hz

on mainline kernel. maximal achievable baudrate is uartclk/16, which is 1.5M in this case of 24MHz

any idea how to reconfigure this uart to use some faster clock on upstream kernel (eg. 48M), so i can achieve 3M baudrate?

 

Currently in device tree the uart1 has following configuration:

clocks = <&clk IMX8MM_CLK_UART1_ROOT>, <&clk IMX8MM_CLK_UART1_ROOT>;
clock-names = "ipg", "per";

Is it possible to change it to use some faster clock? I've read that people use 80MHz instead of 24MHz.

 

Update: it helped to add following:

assigned-clocks = <&clk IMX8MM_CLK_UART1>;
assigned-clock-parents = <&clk IMX8MM_SYS_PLL1_80M>;

 but currently i have DMA disabled and geting occasional data corruption, not sure if that will work correctly. have to try with DMA again, but that caused issues previously.

 

Update 2: with SDMA enabled it does freeze when trying to access the UART.

0 Kudos
Reply

5,699 Views
Harvie
Contributor II

Do you have patch to get UART working reliably on 3M baudrate with upstream kernel?

(5.15.18 or newer)

0 Kudos
Reply