Bus throughput of i.MX8M Mini

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Bus throughput of i.MX8M Mini

Jump to solution
1,987 Views
takayuki_ishii
Contributor V

Hello community,

Our customer hope to know a bus throughput of i.MX8M Mini.

So please suggest following bus width and clock frequency of each bus master peripheral.

1. CPU - AXI switch fabric

2. DDR - AXI switch fablic

3. PCIe - AXI switch fablic

I can found only 2.DDR - AXI.

In reference manual 9.1.1.1 DRAM Interface,

   • 750MHz 128-bit AXI bus

But other 1 and 3 connection of master device can not found.

Do you mind explaining this in more detail?

Best regards,

Ishii.

Labels (1)
0 Kudos
Reply
1 Solution
1,852 Views
igorpadykov
NXP Employee
NXP Employee

Hi Ishii

>But other 1 and 3 connection of master device can not found.

it is the same as described in "9.1.1.1 DRAM Interface", since for interconnections

main NoC is used as central inter-connect fabric, which runs at 750MHz.

>Do you mind explaining this in more detail?

sorry this is internal design information, closed for customers. Please apply

to local NXP office to get more details.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
4 Replies
1,853 Views
igorpadykov
NXP Employee
NXP Employee

Hi Ishii

>But other 1 and 3 connection of master device can not found.

it is the same as described in "9.1.1.1 DRAM Interface", since for interconnections

main NoC is used as central inter-connect fabric, which runs at 750MHz.

>Do you mind explaining this in more detail?

sorry this is internal design information, closed for customers. Please apply

to local NXP office to get more details.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply
1,853 Views
takayuki_ishii
Contributor V

Hello Igor,

Thank you for your response.

>>But other 1 and 3 connection of master device can not found.

 

> it is the same as described in "9.1.1.1 DRAM Interface", since for interconnections

> main NoC is used as central inter-connect fabric, which runs at 750MHz.

Can I get a AXI bus width?

Is it need to ask local FAE?

Best regards,

Ishii.

0 Kudos
Reply
1,853 Views
igorpadykov
NXP Employee
NXP Employee

Hi Ishii

>Can I get a AXI bus width?

>Is it need to ask local FAE?

yes please ask this through local nxp marketing office.

Best regards
igor

0 Kudos
Reply
1,853 Views
takayuki_ishii
Contributor V

Hello Igor,

Thank you for your quick response.

I will ask it to local marketing member.

Best regards,

Ishii.

0 Kudos
Reply