Bus isolation circuit resistor

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Bus isolation circuit resistor

1,423件の閲覧回数
xing
Contributor I

In the  Hardware Development Guide for i.MX7Dual
and 7Solo Applications Processors, it say:

Because only resistors are used, LCD bus loads can
cause current drain, leading to higher (false) supply
current measurements. Each LCD boot signal should
connect to a series resistor to isolate the bus from the
resistors and/or switchers; see Figure 1. Each
configured LCD boot signal sees either a 14.7 kΩ
pulldown or a 4.7 kΩ pullup. For each switch-enabled
pulled-up signal, the supply is presented with a 10 kΩ
current load.
An alternate approach using buffers is implemented in
the SABRE-SD development board design. Either of
these implementations is acceptable.

I want to simplify schematic, can 14.7 kΩ change to 10 kΩ

pastedImage_1.png

I have only three boot configuration, so it change to this

pastedImage_2.png

Is that right ? 

0 件の賞賛
返信
1 返信

1,189件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello

Your scheme is right.

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!

0 件の賞賛
返信