Burn IMX8QXP Android Images problem

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Burn IMX8QXP Android Images problem

1,864 Views
jack_huang1
Contributor IV

        At present, we are verifying Android functions on the NXP IMX8QXP DEMO board (which we got from you), burning and writing according to the steps on ANDROID_USERS_GUIDE.pdf, the following errors will occur. Please help to check the reason (IMX8QXP Linux Images does not have this problem) :

PS D:\Product\IMX8QXP\Android\IMX8QXP_Android_Images> ./uuu_imx_android_flash.bat -f imx8qxp -e

This script is validated with uuu 1.4.182 version, it is recommended to align with this version.

dtbo is supported

dual slot is supported

dynamic partition is supported

vendor_boot is supported

init_boot is supported

generate lines to flash u-boot-imx8qxp.imx to the partition of bootloader0

generate lines to flash partition-table.img to the partition of gpt

generate lines to flash dtbo-imx8qxp.img to the partition of dtbo_a

generate lines to flash vendor_boot.img to the partition of vendor_boot_a

generate lines to flash init_boot.img to the partition of init_boot_a

generate lines to flash boot.img to the partition of boot_a

generate lines to flash vbmeta-imx8qxp.img to the partition of vbmeta_a

generate lines to flash dtbo-imx8qxp.img to the partition of dtbo_b

generate lines to flash vendor_boot.img to the partition of vendor_boot_b

generate lines to flash init_boot.img to the partition of init_boot_b

generate lines to flash boot.img to the partition of boot_b

generate lines to flash vbmeta-imx8qxp.img to the partition of vbmeta_b

generate lines to flash super.img to the partition of super

uuu script generated, start to invoke uuu with the generated uuu script

uuu (Universal Update Utility) for nxp imx chips -- libuuu_1.5.21-0-g1f42172

 

Success 0    Failure 1

 

2:2      1/ 1 [HID(W):LIBUSB_ERROR_IO                ] SDPS: boot -f u-boot-imx8qxp-mek-uuu.imx.link

 

Please check, thank you!

 

0 Kudos
Reply
3 Replies

1,850 Views
Manuel_Salas
NXP TechSupport
NXP TechSupport

Hello @jack_huang1 ,

Please check if your Console/Powershell is in Administrator mode. If yes, please check if the board is in download mode with the command:

uuu -lsusb

If yes, please check the UUU version that you are using.

Other thing to keep in mind, is your board the C0 version or B0 version?

Try again the command:

.\uuu_imx_android_flash.bat -f imx8qxp -e -a

Best regards!

0 Kudos
Reply

1,813 Views
jack_huang1
Contributor IV

Dear:

        The problem has been solved, thank you!

1,820 Views
jackie2
Contributor III

"Please check if your Console/Powershell is in Administrator mode." 

If it is not under Administrator mode, where does u-boot-imx8qxp-mek-uuu.imx.link come from?

 

2:2      1/ 1 [HID(W):LIBUSB_ERROR_IO                ] SDPS: boot -f u-boot-imx8qxp-mek-uuu.imx.link

u-boot-imx8qxp-mek-uuu.imx.link

I also notice the ticket here. 

uuu download Andriod images for imx8qxp mek failed - NXP Community

0 Kudos
Reply