Bulding packages with HardFP

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Bulding packages with HardFP

Jump to solution
1,854 Views
andreygelman
Contributor III

I try to compile Linux with HardFP enabled.

But I cannot find neither prebuilt nor source code for these 2 packages:

- gpu-viv-bin-mx6q-3.0.35-4.0.0

- xserver-xorg-video-imx-viv-3.0.35-4.0.0

Can anyone point me to the right direction ?

Labels (3)
0 Kudos
Reply
1 Solution
1,641 Views
mtx512
Contributor V

Have you checked to see if the binaries are avaliable from the Timesys repo. I checked a few weeks ago and  I'm sure I saw them there.

View solution in original post

0 Kudos
Reply
1 Reply
1,642 Views
mtx512
Contributor V

Have you checked to see if the binaries are avaliable from the Timesys repo. I checked a few weeks ago and  I'm sure I saw them there.

0 Kudos
Reply