Bulding packages with HardFP

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Bulding packages with HardFP

ソリューションへジャンプ
1,797件の閲覧回数
andreygelman
Contributor III

I try to compile Linux with HardFP enabled.

But I cannot find neither prebuilt nor source code for these 2 packages:

- gpu-viv-bin-mx6q-3.0.35-4.0.0

- xserver-xorg-video-imx-viv-3.0.35-4.0.0

Can anyone point me to the right direction ?

ラベル(3)
0 件の賞賛
返信
1 解決策
1,584件の閲覧回数
mtx512
Contributor V

Have you checked to see if the binaries are avaliable from the Timesys repo. I checked a few weeks ago and  I'm sure I saw them there.

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,585件の閲覧回数
mtx512
Contributor V

Have you checked to see if the binaries are avaliable from the Timesys repo. I checked a few weeks ago and  I'm sure I saw them there.

0 件の賞賛
返信