Building yocto using external toolchain?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Building yocto using external toolchain?

ソリューションへジャンプ
13,294件の閲覧回数
Mike1z
Contributor I

Hello,

I'm new to using Yocto, and would like to avoid it's habit of rebuilding the cross compiler each time it runs a clean build.  I have previously successfully built the SDK using 'bitbake meta-toolchain', and installed it to the default location /opt/poky/1.4.1.

I can now use this SDK to build apps external to yocto.  What I want to do is have yocto always use my new pre-built toolchain, instead of recreating gcc each time I perform a build.  I've researched the web, and have seen several people allude to how to solve this problem, but I haven't see an answer yet.

The poky handbook says

"Using the external toolchains is simply a case of untarring the tarball into the root of your system (it only creates files in /usr/local/poky) and then enabling the option in local.conf. "

But it doesn't tell you how... :smileysad:.  Anybody know how to do this?

ラベル(2)
タグ(3)
1 解決策
6,034件の閲覧回数
daiane_angolini
NXP Employee
NXP Employee

In my opinion, you don´t need to care about "re-building" gcc each time you have a new clean build.

The option given to you to use an external toolchain with yocto, gives you the power to actually choose which *other* toolchain you want, for example, the linaro one.

So, if you really want a *different* toolchain, I think you should work to use an external toolchain.

But, in other hand, if you only complain that build time take too much, there are other things you may change on your configuration in order to try to reduce this time.

Yocto always create a folder with the "pre-built" binaries from each package, it´s called sstate-cache. You can share this folder with your other build folders, or even with your co-workers. (https://www.yoctoproject.org/docs/current/poky-ref-manual/poky-ref-manual.html#var-SSTATE_DIR)

In my personal opinion, you should not use the meta-toolchain as "external" toolchain, you should use yocto toolchain "as-is", if you´re using an stable branch it will only be changed in case of a bugfix, and I think you want bugfixes.

Please, apologize my delay, I´ve been busy with meta-fsl-arm release these past days.... And please,  let me know your thoughts.

元の投稿で解決策を見る

4 返答(返信)
6,035件の閲覧回数
daiane_angolini
NXP Employee
NXP Employee

In my opinion, you don´t need to care about "re-building" gcc each time you have a new clean build.

The option given to you to use an external toolchain with yocto, gives you the power to actually choose which *other* toolchain you want, for example, the linaro one.

So, if you really want a *different* toolchain, I think you should work to use an external toolchain.

But, in other hand, if you only complain that build time take too much, there are other things you may change on your configuration in order to try to reduce this time.

Yocto always create a folder with the "pre-built" binaries from each package, it´s called sstate-cache. You can share this folder with your other build folders, or even with your co-workers. (https://www.yoctoproject.org/docs/current/poky-ref-manual/poky-ref-manual.html#var-SSTATE_DIR)

In my personal opinion, you should not use the meta-toolchain as "external" toolchain, you should use yocto toolchain "as-is", if you´re using an stable branch it will only be changed in case of a bugfix, and I think you want bugfixes.

Please, apologize my delay, I´ve been busy with meta-fsl-arm release these past days.... And please,  let me know your thoughts.

6,034件の閲覧回数
manjunathjoshi
Contributor V

Hello Daiane,

Can you elaborate where exactly the changes have to made?

i am building YOCTO with poky distribution but i want linaro as external toolchain.

Regards,

Manju

0 件の賞賛
返信
6,034件の閲覧回数
daiane_angolini
NXP Employee
NXP Employee

Mainly local.conf

There how-to's from Linaro community showing how to configure it. It's something like adding 3 lines to your local.conf, and untar the linaro toolchain in a known place.

I prefer you take the Linaro community how-to, this way it's the most updated version.

0 件の賞賛
返信
6,034件の閲覧回数
manjunathjoshi
Contributor V

Hello Daiane,

Thank you for your immediate reply.

I added following lines in local.conf,

TCLIBC = "external-linaro-toolchain"

TCMODE = "external-linaro"

EXTERNAL_TOOLCHAIN = " /home/manjunath/linaro/gcc-linaro-arm-linux-gnueabihf-4.7-2013.01-20130125_linux/"

and i had to add .inc files for tclibc , tcmode and version in sources/poky/meta/conf/distro/include/

Manju