Building the image

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Building the image

1,093 次查看
unaigonzalez
Contributor II

Hello,

I am working with i.mx28. I am trying to build a kernel with a new

configuration, so, following your step by step guide I saw that the resulting

file is not complete.

The point is, that after I build with ./ltib command, I expect to have a big

rootfs.ext2 as image, but I only have a 11Mbit file. When I use CF Imager

to set up my SD and I use it on the i.mx28, the error: Kernel panic appear.

标签 (1)
0 项奖励
回复
1 回复

970 次查看
Yuri
NXP Employee
NXP Employee

  Please look at my comments below.

1.
  Default build configuration is minimal, so the rootfs is not big.

Please select  LTIB configuration as FSL_gnome, for example.

2.

Please try the mfg tool to deploy the image to Your board.

3.
  If Your board and i.MX28 EVK differ - it may cause kernel panic.


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复