Building the image

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Building the image

1,583件の閲覧回数
unaigonzalez
Contributor II

Hello,

I am working with i.mx28. I am trying to build a kernel with a new

configuration, so, following your step by step guide I saw that the resulting

file is not complete.

The point is, that after I build with ./ltib command, I expect to have a big

rootfs.ext2 as image, but I only have a 11Mbit file. When I use CF Imager

to set up my SD and I use it on the i.mx28, the error: Kernel panic appear.

ラベル(1)
0 件の賞賛
返信
1 返信

1,460件の閲覧回数
Yuri
NXP Employee
NXP Employee

  Please look at my comments below.

1.
  Default build configuration is minimal, so the rootfs is not big.

Please select  LTIB configuration as FSL_gnome, for example.

2.

Please try the mfg tool to deploy the image to Your board.

3.
  If Your board and i.MX28 EVK differ - it may cause kernel panic.


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信