I have build images for imx53EVK board using yocto updated at https://community.freescale.com/message/570496#570496 and flashed images by referring https://community.freescale.com/message/528720#528720 .
When I flashed the u-boot built with yocto then board is not booting, but if I use prebuilt u-boot then board is booting.
Now I want to build VPU and gstreamer using Yocto.
I could see the following line in sources/Documentation/release-notes/source/issues-known.rst file inside yocto.
--------------------------------------------------------------------------------------------------------------
1. Fail to build imx-lib/imx-vpu/imx-test/gst-fsl-plugin when building against linux-fslc
--------------------------------------------------------------------------------------------------------------
Any one tried to build imx-vpu and gstreamer using yocto?
I thought of building vpu first. I could see following package entry in meta-fsl-arm/recipes-multimedia/libfslcodec/libfslcodec.inc file.
----------------------------------------------------------------------------------
PACKAGECONFIG[vpu] = "--enable-vpu,--disable-vpu,imx-vpu"
----------------------------------------------------------------------------------
I think it has to be enabled in the poky.conf(as the distribution is poky from local.conf). Can you please suggest me how to make an entry in poky.conf to enable vpu.
I started building gstreamer by adding following content in local.conf file.
IMAGE_INSTALL_append = "\
gstreamer \
gst-meta-base \
gst-plugins-bad \
gst-fsl-plugin"
It build successfully, but when I execute following command, it is giving "WARNING: erroneous pipeline: no element "aiurdemux"" error.
#gst-launch filesrc location=Avengers.mp4 typefind=true ! aiurdemux ! queue max-size-time=0 ! mfw_vpudecoder ! mfw_v4lsink
I thought the error related to "aiurdemux" may be related to absence of gst-ugly plugins, so I tried building gst-ugly plugins, but build is failing with following error.
----------------------------------------------------------------------------
NOTE: Resolving any missing task queue dependencies
ERROR: Nothing RPROVIDES 'gst-plugins-ugly' (but /home/user/fido/fsl-community-bsp/sources/poky/meta/recipes-core/images/core-image-minimal.bb RDEPENDS on or otherwise requires it)
ERROR: gst-plugins-ugly was skipped: because it has a restricted license not whitelisted in LICENSE_FLAGS_WHITELIST
NOTE: Runtime target 'gst-plugins-ugly' is unbuildable, removing...
Missing or unbuildable dependency chain was: ['gst-plugins-ugly']
ERROR: Required build target 'core-image-minimal' has no buildable providers.
Missing or unbuildable dependency chain was: ['core-image-minimal', 'gst-plugins-ugly']
---------------------------------------------------------------------------
Can you please help to fix the following error.
WARNING: erroneous pipeline: no element "aiurdemux"
Please, take a loon in
FSL Community BSP Release Notes 1.8 documentation
and
Are you subscribed to meta-freescale mailing list? Several important changes were included recently for mx53 and we discussed all them in meta-freescale. Maybe you can take a look on archives.
I was not able to understand which source code and branch are you using.