How to enable sgtl5000 in android kitkat with imx6q?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

How to enable sgtl5000 in android kitkat with imx6q?

2,302 次查看
conteczxy
Contributor III

Hi, I am porting sgtl5000 drivers to android 4.4.2, and there is still no sound, and when selecting from Setting->Sound->notification sound menu, some error shows in logcat,

log as below:

---------

11-24 18:06:23.850: W/AudioPolicyManagerBase(2319): getOutput() could not find output for stream 1, samplingRate 0,format 0, channels 3, flags 0

11-24 18:06:23.850: W/AudioPolicyManagerBase(2319): getOutput() could not find output for stream 1, samplingRate 0,format 0, channels 3, flags 0

11-24 18:06:23.850: W/AudioPolicyManagerBase(2319): getOutput() could not find output for stream 1, samplingRate 48000,format 1, channels 3, flags 4

11-24 18:06:23.850: E/AudioTrack(2700): Could not get audio output for stream type 1

11-24 18:06:23.850: E/SoundPool(2700): Error creating AudioTrack

11-24 18:06:23.900: D/Ringtone(2957): Successfully created local player

11-24 18:06:23.900: E/AudioPolicyManagerBase(2319): getDeviceForStrategy() speaker device not found for STRATEGY_SONIFICATION

11-24 18:06:23.900: W/AudioPolicyManagerBase(2319): getOutput() could not find output for stream 5, samplingRate 0,format 0, channels 3, flags 0

11-24 18:06:23.900: E/MediaPlayer(2957): error (-19, 0)

11-24 18:06:23.900: E/MediaPlayer(2957): Should have subtitle controller already set

11-24 18:06:23.900: E/MediaPlayer(2957): Error (-19,0)

Some days ago,  I made similar porting steps in android4.3, it works well, but it is not applicable to android4.4.

Where is the problem?  Any suggestion is appreciated.

Thanks.

标签 (2)
标记 (4)
0 项奖励
回复
2 回复数

1,372 次查看
conteczxy
Contributor III

I found config_sgtl5000.h was missing in the dir "hardware/imx/alsa",

and tinyalsa_hal.c should be made some changes.

-------

#include "config_sgtl5000.h"

... ...

struct audio_card *audio_card_list[SUPPORT_CARD_NUM] = {

   &sgtl5000_card,

    &wm8958_card,

    &wm8962_card,

    &hdmi_card,

    &usbaudio_card,

    &spdif_card,

    &null_card,

};

0 项奖励
回复

1,372 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Xiyuan

please look at boundarydevices android 4.4.2 (based on FSL release) it includes sgtl5000

support

https://boundarydevices.com/android-kitkat-second-release-mx6-boards/

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------