Hello everyone,
I have u-boot and kernel. I want to create a Rootfs from yocto.
I download all files with Mfg tool to my board. Everything work good.
But when I run my GUI app, I can not see Turkish and Chinese characters.
How can i add these?
I have to make some modifications, but in kernel or in rootfs.. I dont know this.
Please may you help me?
Thank you for your support.
Have a nice day.
Solved! Go to Solution.
 joanxie
		
			joanxie
		
		
		
		
		
		
		
		
	
			
		
		
			
					
		you also can refer to this customer:
 joanxie
		
			joanxie
		
		
		
		
		
		
		
		
	
			
		
		
			
					
		my test steps:
1put this package to  /usr/lib/fonts 
 then in the imxplayer, pls choose wenquanyi micro hei
2) cp /usr/lib/fonts/wqy-microhei.ttc /usr/share/fonts/ttf/ 
 fc-list 
 gst-launch-1.0 playbin flags=0x17 subtitle-font-desc="WenQuanYi Micro Hei  Regular 14" uri=file://。。。。。。。
Hello Joan Xie,
Thanks for your big support.
Everything is perfect now.
I have Chinese and Turkish charcters.
Thanks again. :smileyhappy:
 joanxie
		
			joanxie
		
		
		
		
		
		
		
		
	
			
		
		
			
					
		try to use the steps to add chinese character: (the example for mx6ul board)
Modify configuration to support Chinese character set.
$ source setup-environment imx6ul-build-directory
$ cd conf
$ vi local.conf ;add the following two lines to support Chinese in the end
GLIBC_GENERATE_LOCALES = "zh_CN.UTF-8 en_GB.UTF-8 en_US.UTF-8"
IMAGE_LINGUAS ?= "zh-cn"
$ cd .. && bitbake fsl-image-gui
burn the new image to your board
Boot up your i.mx6ul-EVK board and copy wenquanyi.ttf to /usr/share/fonts/ttf/
# cd /usr/share/fonts/ttf
# rz ; then select wenquanyi.ttf as z-modem received file
# fc-cache -lv
5. Add LANG=zh_CN.UTF-8 in your environment varialbe
# vi /etc/profile ;add the following line in the end
export LANG=zh_CN.UTF-8
Hello Joan Xie,
Thanks for your reply.
I did these steps, I had an image with Turkish and Chinese languages but There are no Turkish characters on the my GUI.
Do you have any suggestion about this?
Thank you very much. Best regards.
 joanxie
		
			joanxie
		
		
		
		
		
		
		
		
	
			
		
		
			
					
		I don't have Turkish characters package, I think the same steps as chinese character, if you have, put the same path as chinese character.
Hello Joan Xie,
Thanks for your reply to my question.
I did your steps, but on my gui (it was created at qt creator) I can not see chinese characters. I run my gui at my Ubuntu desktop PC, I can see all Chinese charcters. I read all text from XML file on my gui. Maybe I write wrong TTF name in XML file.
Also I did not do this steps.
# rz ; then select wenquanyi.ttf as z-modem received file
# fc-cache -lv
I generate my own rootfs, But there is not rz command.. This is important?
wenquanyi ttf's name is "WenQuanYi Micro Hei" or it is only WenQuanYi?
I added a package for rz command. I wrote "rz" command in /usr/share/fonts/ttf directory.
It takes a few minutes. But it is running... I am waiting for this..
 joanxie
		
			joanxie