Build system - without Yatco - Link is required.

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Build system - without Yatco - Link is required.

938 次查看
maheshkalmeshwa
Contributor I

Hay All,

I am seeking out where is link to get all the source (Boot loader ,Linux Kernel, File system and toolchain application gsteramer1.0) and readMe Documnets to bulid all.

If i get tar file or Git is fine with me but i do not need yocto build system.

Am using IM6x Nitrogen hardware.

Regards

MK

标记 (1)
0 项奖励
回复
1 回复

869 次查看
Rita_Wang
NXP TechSupport
NXP TechSupport

Hi ,

The IM6x Nitrogen is the third company board, you can go to https://boundarydevices.com/product/sabre-lite-imx6-sbc/  ask for help. Hope this can help you .
Have a great day,
Rita

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Mark Correct button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复