Build system - without Yatco - Link is required.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Build system - without Yatco - Link is required.

1,370件の閲覧回数
maheshkalmeshwa
Contributor I

Hay All,

I am seeking out where is link to get all the source (Boot loader ,Linux Kernel, File system and toolchain application gsteramer1.0) and readMe Documnets to bulid all.

If i get tar file or Git is fine with me but i do not need yocto build system.

Am using IM6x Nitrogen hardware.

Regards

MK

タグ(1)
0 件の賞賛
返信
1 返信

1,301件の閲覧回数
Rita_Wang
NXP TechSupport
NXP TechSupport

Hi ,

The IM6x Nitrogen is the third company board, you can go to https://boundarydevices.com/product/sabre-lite-imx6-sbc/  ask for help. Hope this can help you .
Have a great day,
Rita

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Mark Correct button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信