Broadcom bluetooth driver bcm_dhd 1363 error in imx8 kernel 4.9.51

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Broadcom bluetooth driver bcm_dhd 1363 error in imx8 kernel 4.9.51

1,988 次查看
nsyed
Contributor I

HI

, I am using imx8 based board from compulab

CL-SOM-iMX8 | NXP i.MX 8 | System-on-Module | Computer-on-Module | CompuLab 

Its using 4.9.51 kernel which i got from source.codeaurora.org/external/imx/linux-imx -b imx_4.9.51_imx8mq

Then I applied real time path from preempt_RT website which was patch-4.9.47-rt37.patch and thats the closest one i found with 4.9.51 kernel.

The patch is applied Ok but after that when I do make it complains about broadcom driver (Wifi + Bluetooth) .

here is the error message

============================================================================

CC [M] drivers/gpu/drm/nouveau/nvkm/engine/ce/gk104.o
drivers/net/wireless/bcmdhd_1363/dhd_pno.c: In function ‘_dhd_pno_get_for_batch’:
drivers/net/wireless/bcmdhd_1363/dhd_pno.c:3045:23: error: passing argument 1 of ‘waitqueue_active’ from incompatible pointer type [-Werror=incompatible-pointer-types]
if (waitqueue_active(&_pno_state->get_batch_done.wait))
^
In file included from ./include/linux/uprobes.h:30:0,
from ./include/linux/mm_types.h:13,
from ./include/linux/sched.h:27,
from ./arch/arm64/include/asm/compat.h:25,
from ./arch/arm64/include/asm/stat.h:23,
from ./include/linux/stat.h:5,
from ./include/linux/module.h:10,
from drivers/net/wireless/bcmdhd_1363/include/linuxver.h:55,
from drivers/net/wireless/bcmdhd_1363/include/linux_osl.h:250,
from drivers/net/wireless/bcmdhd_1363/include/osl.h:49,
from drivers/net/wireless/bcmdhd_1363/dhd_pno.c:37:
./include/linux/wait.h:136:19: note: expected ‘wait_queue_head_t * {aka struct __wait_queue_head *}’ but argument is of type ‘struct swait_queue_head *’
static inline int waitqueue_active(wait_queue_head_t *q)
^~~~~~~~~~~~~~~~
drivers/net/wireless/bcmdhd_1363/dhd_pno.c: In function ‘dhd_pno_event_handler’:
drivers/net/wireless/bcmdhd_1363/dhd_pno.c:3801:25: error: passing argument 1 of ‘waitqueue_active’ from incompatible pointer type [-Werror=incompatible-pointer-types]
if (!waitqueue_active(&_pno_state->get_batch_done.wait)) {
^
In file included from ./include/linux/uprobes.h:30:0,
from ./include/linux/mm_types.h:13,
from ./include/linux/sched.h:27,
from ./arch/arm64/include/asm/compat.h:25,
from ./arch/arm64/include/asm/stat.h:23,
from ./include/linux/stat.h:5,
from ./include/linux/module.h:10,
from drivers/net/wireless/bcmdhd_1363/include/linuxver.h:55,
from drivers/net/wireless/bcmdhd_1363/include/linux_osl.h:250,
from drivers/net/wireless/bcmdhd_1363/include/osl.h:49,
from drivers/net/wireless/bcmdhd_1363/dhd_pno.c:37:
./include/linux/wait.h:136:19: note: expected ‘wait_queue_head_t * {aka struct __wait_queue_head *}’ but argument is of type ‘struct swait_queue_head *’
static inline int waitqueue_active(wait_queue_head_t *q)
^~~~~~~~~~~~~~~~
CC drivers/net/ethernet/intel/igbvf/mbx.o
CC [M] drivers/gpu/drm/nouveau/nvkm/engine/ce/gm107.o
CC [M] drivers/net/usb/asix_devices.o
CC drivers/net/ethernet/intel/igbvf/ethtool.o
CC [M] drivers/gpu/drm/nouveau/nvkm/engine/ce/gm200.o
cc1: some warnings being treated as errors
make[4]: *** [drivers/net/wireless/bcmdhd_1363/dhd_pno.o] Error 1
make[3]: *** [drivers/net/wireless/bcmdhd_1363] Error 2
make[2]: *** [drivers/net/wireless] Error 2

Please advise how this error can be fixed

Many thanks

0 项奖励
回复
1 回复

1,733 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Nabeel

NXP i.MX8M official bsp supports Murata 1CQ (QCA6174A) as described on Table 9. Supported features

attached Release Notes, seems this may be posted on relevant mail list:

realtime:communication:mailinglists [Linux Foundation Wiki] 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复