Bring up custom imx8qm board with uuu (based on mek)

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Bring up custom imx8qm board with uuu (based on mek)

1,628 次查看
miners
Contributor II

We have a custom board based off of the MCIMX8QM-CPU MEK Platform. We are trying to bring it up using that image as provided by NXP just to get a bootable unit.

When attempting to use the UUU tool it repeatedly tries to load the boot file until it is cancelled with ctrl+c as shown in the image below. We currently are not sure if our UART that is connected to the imx8 is working (it is routed through an FPGA that, while programmed, is not vetted), but we don't see anything on that connection when viewed at 115200,8,n,1.

Does this point to anything obvious in the bring up process?

Thanks

miners_0-1697839125370.png

Contents of uuu.auto-imx8qmmek

uuu_version 1.2.39

# This command will be run when i.MX6/7 i.MX8MM, i.MX8MQ
SDP: boot -f imx-boot-imx8qmmek-sd.bin-flash

# This command will be run when ROM support stream mode
# i.MX8QXP, i.MX8QM
SDPS: boot -f imx-boot-imx8qmmek-sd.bin-flash

# These commands will be run when use SPL and will be skipped if no spl
# SDPU will be deprecated. please use SDPV instead of SDPU
# {
SDPU: delay 1000
SDPU: write -f imx-boot-imx8qmmek-sd.bin-flash -offset 0x57c00
SDPU: jump
# }

# These commands will be run when use SPL and will be skipped if no spl
# if (SPL support SDPV)
# {
SDPV: delay 1000
SDPV: write -f imx-boot-imx8qmmek-sd.bin-flash -skipspl
SDPV: jump
# }

FB: ucmd setenv fastboot_dev mmc
FB: ucmd setenv mmcdev ${emmc_dev}
FB: ucmd mmc dev ${emmc_dev}
FB: flash -raw2sparse all imx-image-multimedia-imx8qmmek.wic
FB: flash bootloader imx-boot-imx8qmmek-sd.bin-flash
FB: ucmd if env exists emmc_ack; then ; else setenv emmc_ack 0; fi;
FB: ucmd mmc partconf ${emmc_dev} ${emmc_ack} 1 0
FB: done

 

标记 (1)
0 项奖励
回复
4 回复数

1,568 次查看
miners
Contributor II

Looking at dmesg after each run I am seeing the following, 

 

[3260423.853655] usb 1-3: USB disconnect, device number 27
[3260424.103792] usb 1-3: new high-speed USB device number 28 using xhci_hcd
[3260424.484613] usb 1-3: Device not responding to setup address.
[3260424.688821] usb 1-3: Device not responding to setup address.
[3260424.896781] usb 1-3: device not accepting address 28, error -71
[3260425.212828] usb 1-3: new high-speed USB device number 29 using xhci_hcd
[3260425.326630] usb 1-3: Device not responding to setup address.
[3260425.528516] usb 1-3: Device not responding to setup address.
[3260425.736541] usb 1-3: device not accepting address 29, error -71
[3260425.736682] usb usb1-port3: attempt power cycle
[3260426.116769] usb 1-3: new high-speed USB device number 30 using xhci_hcd
[3260426.116818] usb 1-3: Device not responding to setup address.
[3260426.320804] usb 1-3: Device not responding to setup address.
[3260426.528472] usb 1-3: device not accepting address 30, error -71
[3260427.260557] usb 1-3: new high-speed USB device number 31 using xhci_hcd
[3260427.260609] usb 1-3: Device not responding to setup address.
[3260427.464786] usb 1-3: Device not responding to setup address.
[3260427.672720] usb 1-3: device not accepting address 31, error -71
[3260427.672801] usb usb1-port3: unable to enumerate USB device
[3260427.894791] usb 1-3: new high-speed USB device number 32 using xhci_hcd
[3260428.021405] usb 1-3: New USB device found, idVendor=1fc9, idProduct=0129, bcdDevice= 0.02
[3260428.021429] usb 1-3: New USB device strings: Mfr=1, Product=2, SerialNumber=0
[3260428.021436] usb 1-3: Product: SE Blank 8QM 
[3260428.021440] usb 1-3: Manufacturer: NXP       SemiConductor Inc 
[3260428.024462] hid-generic 0003:1FC9:0129.01C8: hiddev96,hidraw0: USB HID v1.10 Device [NXP       SemiConductor Inc  SE Blank 8QM ] on usb-0000:00:14.0-3/input0
0 项奖励
回复

1,593 次查看
Harvey021
NXP TechSupport
NXP TechSupport

Firstly, would recommend to use dd to burn the image to sd card to check if there is something wrong with the image. if fine with the image, then check the uart hardware.

 

Best regards

Harvey

0 项奖励
回复

1,585 次查看
miners
Contributor II

There is no SD card, just an on-board eMMC and flash device. 

We tried other board images with uuu and they all fail the boot step immediately with,

LIBUSB_IO_ERROR

the fact that this one gets past that and is the image based on the board we referenced the design after seems promising. 

Attempting with an images based on a different dev board,

miners_0-1698075853968.png

 

0 项奖励
回复

1,370 次查看
jsmith8831
Contributor III

@miners, I'm experiencing the same issue.  Did you happen to resolve the problem?  It appears as though the USB is re-enumerating as soon as the first command is ran.  SDPS: boot -f flash.bin

0 项奖励
回复