Dear;
Currently NXP IMX93, model is PIMX9352CVUXMAA, software BSP version is Linux 6.1.22_2.0.0, storage uses LPDDR4+EMMC configuration, EMMC model is SDINBDG4-16G-XI1; When UUU is used to write uboot, run the uuu -V -b emmc flash.bin command. If the MMC cannot be identified, the following information is displayed:
U-Boot SPL 2023.04-lf_v2023.04+g6b39c4f44 (Dec 09 2023 - 06:56:58 +0000)
SOC: 0xa0009300
LC: 0x40010
M33 prepare ok
Normal Boot
Trying to boot from BOOTROM
Boot Stage: USB boot
Find img info 0x88000000, size 416
Download 1654784, Total size 1655808
NOTICE: BL31: v2.8(release):automotive-13.0.0_2.1.0-0-g99195a23d
NOTICE: BL31: Built : 06:14:17, Jun 2 2023
U-Boot 2023.04-lf_v2023.04+g6b39c4f44 (Dec 09 2023 - 06:56:58 +0000)
CPU: i.MX93(52) rev1.0 1700 MHz (running at 1692 MHz)
CPU: Consumer temperature grade (0C to 95C) at 32C
Reset cause: WDOG3 (0x21)
Model: VT SBC SMARC IMX93 CB board
DRAM: 2 GiB
tcpc_init: Can't find device id=0x52
setup_typec: tcpc portpd init failed, err=-19
tcpc_init: Can't find device id=0x51
setup_typec: tcpc port2 init failed, err=-19
tcpc_init: Can't find device id=0x50
setup_typec: tcpc port1 init failed, err=-19
pca953x gpio@22: Error reading output register
Core: 219 devices, 32 uclasses, devicetree: separateVT102 | 脱机 | ttyUSB0
MMC: FSL_SDHC: 0, FSL_SDHC: 1
Loading Environment from nowhere... OK
[*]-Video Link 0adv7535_mipi2hdmi hdmi@3d: Can't find cec device id=0x3c
fail to probe panel device hdmi@3d
fail to get display timings
probe video device failed, ret -19
[0] lcd-controller@4ae30000, video
[1] dsi@4ae10000, video_bridge
[2] hdmi@3d, panel
adv7535_mipi2hdmi hdmi@3d: Can't find cec device id=0x3c
fail to probe panel device hdmi@3d
fail to get display timings
probe video device failed, ret -19
In: serial
Out: serial
Err: serial
BuildInfo:
- ELE firmware version 0.0.10-af252062
MMC: no card present
UID: 0x3dc76249 0x234933d1 0x2bff409f 0xbf0d0444
Detect USB boot. Will enter fastboot mode!
Net: pca953x gpio@22: Error reading output register
Is LPDDR4 not configured at present the cause of the problem? Excuse me: Is there any IMX93 debugging guide documentation?
Thanks!
Best Regards!
If the board can't detect the MMC, it can't flash the firmware.
MMC: no card present
-->Does this problem occur all the time or occasionally? This is a very critical issue.
Dears;
At present, it has been verified on the development board of Feiling that all are normal, and my own board has just been welded and debutted, and it is found that EMMC cannot be recognized, resulting in no burning, which is being excluded.
Best Regards!