Booting the system using interrupt

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Booting the system using interrupt

1,813 Views
sadatanvashisth
Contributor II

Can I use any external interrupt to turn the  processor IMX6UL ON after power off, with out using ON/OFF pin?

Regards,

Sadatan

Labels (1)
0 Kudos
Reply
3 Replies

1,740 Views
igorpadykov
NXP Employee
NXP Employee

Hi Sadatan

unfortunately not.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

1,740 Views
sadatanvashisth
Contributor II

Can I utilize one of the temper pin to detect the a high voltage in OFF condition and then using other temper pin provide a pulse on ONOFF pin to turn the PMIC ON?

0 Kudos
Reply

1,740 Views
igorpadykov
NXP Employee
NXP Employee

Hi Sadatan

 

unfortunately not.

 

Best regards
igor

0 Kudos
Reply