Booting the system using interrupt

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Booting the system using interrupt

1,807件の閲覧回数
sadatanvashisth
Contributor II

Can I use any external interrupt to turn the  processor IMX6UL ON after power off, with out using ON/OFF pin?

Regards,

Sadatan

ラベル(1)
0 件の賞賛
返信
3 返答(返信)

1,734件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Sadatan

unfortunately not.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

1,734件の閲覧回数
sadatanvashisth
Contributor II

Can I utilize one of the temper pin to detect the a high voltage in OFF condition and then using other temper pin provide a pulse on ONOFF pin to turn the PMIC ON?

0 件の賞賛
返信

1,734件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Sadatan

 

unfortunately not.

 

Best regards
igor

0 件の賞賛
返信