Booting suspends.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Booting suspends.

1,524 Views
ernestlih
Contributor II

Hello,

My own board has been designed with i.MX8MQ running qt image compiled in 4.14.78.

It has 2GB memory.

Booting process sometimes suspends at 'Started Start Psplash Boot Screen' and doesn't go further.

Sometimes kernel panic occurs.

I wonder whether it is memory timing issue or other issue.

Can you advise what the problem is?

Screenshot from 2019-12-03 14-55-26.png

Screenshot from 2019-12-03 14-59-57.png

Regards,

Ernest

0 Kudos
Reply
1 Reply

1,490 Views
igorpadykov
NXP Employee
NXP Employee

Hi Ernest

one can try to run latest ddr test https://community.nxp.com/docs/DOC-340179 

and follow Chapter 4 How to bring up a new MX8MSCALE board MSCALE_DDR_Tool_User_Guide.pdf
included in ddr test package. Use latest Linux L4.19.35   Linux_4.19.35_1.1.0_ga
linux-imx - i.MX Linux kernel 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply