Booting suspends.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Booting suspends.

1,520件の閲覧回数
ernestlih
Contributor II

Hello,

My own board has been designed with i.MX8MQ running qt image compiled in 4.14.78.

It has 2GB memory.

Booting process sometimes suspends at 'Started Start Psplash Boot Screen' and doesn't go further.

Sometimes kernel panic occurs.

I wonder whether it is memory timing issue or other issue.

Can you advise what the problem is?

Screenshot from 2019-12-03 14-55-26.png

Screenshot from 2019-12-03 14-59-57.png

Regards,

Ernest

0 件の賞賛
返信
1 返信

1,486件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Ernest

one can try to run latest ddr test https://community.nxp.com/docs/DOC-340179 

and follow Chapter 4 How to bring up a new MX8MSCALE board MSCALE_DDR_Tool_User_Guide.pdf
included in ddr test package. Use latest Linux L4.19.35   Linux_4.19.35_1.1.0_ga
linux-imx - i.MX Linux kernel 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信