Booting IMXRT1170

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Booting IMXRT1170

Jump to solution
2,006 Views
TM_MI
Contributor III

Hello,

For our customized board I would like to verify the booting process. I understand that the boot mode has to be 10 for internal mode; FlexSPI 1 in boot configuration and it is basically booting from the QSPI Flash (S25WP128-JBLE) but what is the use of the Octal Flash here (MX25UM51345GXDI00) ?

If I am correct the application has to be downloaded the first time using J-Link and serial download mode (01) to the QSPI Flash; booting configuration are not required to be changed for Jtag connection.

For our board we are also looking to boot from serial download (01) into the NAND Flash using USB OTG1 or UART and MCU BootUtility ? is this Possible?

Thank you,

TM

0 Kudos
Reply
1 Solution
1,990 Views
jeremyzhou
NXP Employee
NXP Employee

Hi,
Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
1) FlexSPI 1 in boot configuration and it is basically booting from the QSPI Flash (S25WP128-JBLE) but what is the use of the Octal Flash here (MX25UM51345GXDI00)
-- The RT MCU can boot from the Octal Flash besides QSPI flash.
2) If I am correct the application has to be downloaded the first time using J-Link and serial download mode (01) to the QSPI Flash; booting configuration are not required to be changed for Jtag connection.
-- No, I don't think so.
3) For our board we are also looking to boot from serial download (01) into the NAND Flash using USB OTG1 or UART and MCU BootUtility ? is this Possible?
-- Yes, it's possible.
Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
1,991 Views
jeremyzhou
NXP Employee
NXP Employee

Hi,
Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
1) FlexSPI 1 in boot configuration and it is basically booting from the QSPI Flash (S25WP128-JBLE) but what is the use of the Octal Flash here (MX25UM51345GXDI00)
-- The RT MCU can boot from the Octal Flash besides QSPI flash.
2) If I am correct the application has to be downloaded the first time using J-Link and serial download mode (01) to the QSPI Flash; booting configuration are not required to be changed for Jtag connection.
-- No, I don't think so.
3) For our board we are also looking to boot from serial download (01) into the NAND Flash using USB OTG1 or UART and MCU BootUtility ? is this Possible?
-- Yes, it's possible.
Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply